Wired Connection Setup

Next Generation Control Mill Operator's Manual

The Online Interactive Operator's Manual is currently available in English only.

A PDF version of the Operator's Manual is available for download in multiple languages. Click the link below to view the Operator's Manual in your language. Click "Continue" to view the online version in English.

Get a translated PDF Download Continue

Before you begin, ask your network administrator if your network has a Dynamic Host Configuration Protocol (DHCP) server. If it does not have a DHCP server, collect this information:

  • The IP address that your machine will use on the network
  • The Subnet Mask address
  • The Default Gateway address
  • The DNS Server name
  1. Connect an active Ethernet cable to the Ethernet port on your machine.
  2. Select the Wired Connection tab in the Network tabbed menu.
  3. Change the Wired Network Enabled setting to ON.
  4. If your network has a DHCP server, you can let the network assign an IP address automatically. Change the Obtain Address Automatically setting to ON, and then press F4 to complete the connection. If your network does not have a DHCP server, go to the next step.
  5. Type the machine’s IP Address, the Subnet Mask address, the Default Gateway address, and the DNS Server name into their respective fields.
  6. Press F4 to complete the connection, or press F3 to discard your changes.

After the machine successfully connects to the network, the Status indicator in the Wired Network Information box changes to UP.

Be aware: Many service and repair procedures should be done only by authorized personnel. The service technicians at your Haas Factory Outlet (HFO) have the training, experience, and are certified to do these tasks safely and correctly. You should not do machine repair or service procedures unless you are qualified and knowledgeable about the processes.

Danger: Some service procedures can be dangerous or life-threatening. DO NOT attempt a procedure that you do not completely understand. Contact your Haas Factory Outlet (HFO) and schedule a service technician visit if you have any doubts about doing a procedure.

Feedback