Setting Part Zero Offset

Classic Control - Mill Operator's Manual

The Online Interactive Operator's Manual is currently available in English only.

A PDF version of the Operator's Manual is available for download in multiple languages. Click the link below to view the Operator's Manual in your language. Click "Continue" to view the online version in English.

Get a translated PDF Download Continue

In order to machine a workpiece (part), the mill needs to know where the part is located on the table. You can use an edge finder, an electronic probe, or many other tools and methods to establish part zero. To set the part zero offset with a mechanical pointer:

Part Zero Set

  1. Place the material [1] in the vise and tighten.
  2. Load a pointer tool [2] in the spindle.
  3. Press HANDLE JOG [E].
  4. Press .1/100. [F] (The mill will move at a fast speed when the handle is turned).
  5. Press +Z [A].
  6. Handle jog [J] the Z-Axis approximately 1" above the part.
  7. Press .001/1. [G] (The mill will move at a slow speed when the handle is turned).
  8. Handle jog [J] the Z-Axis approximately. 0.2" above the part.
  9. Select between the X and Y axes [I] and handle jog [J] the tool to the upper left corner of the part (See illustration [9]).
  10. Press OFFSET [C] until the Active Work Offset pane is active.
  11. Cursor [H] to G54 X-Axis column.
  12. caution: In the next step, do not press PART ZERO SET a third time; this loads a value into the Z Axis column. This causes a crash or a Z-Axis alarm when the program is run.
    Press PART ZERO SET [B] to load the value into the X-Axis column. The second press of PART ZERO SET [B] loads the value into the Y-Axis column.

Be aware: Many service and repair procedures should be done only by authorized personnel. The service technicians at your Haas Factory Outlet (HFO) have the training, experience, and are certified to do these tasks safely and correctly. You should not do machine repair or service procedures unless you are qualified and knowledgeable about the processes.

Danger: Some service procedures can be dangerous or life-threatening. DO NOT attempt a procedure that you do not completely understand. Contact your Haas Factory Outlet (HFO) and schedule a service technician visit if you have any doubts about doing a procedure.

Feedback