Setting Aliases

Next Generation Control Mill Operator's Manual

The Online Interactive Operator's Manual is currently available in English only.

A PDF version of the Operator's Manual is available for download in multiple languages. Click the link below to view the Operator's Manual in your language. Click "Continue" to view the online version in English.

Get a translated PDF Download Continue

The G-code or M-code alias setup is done on the Alias Codes window. To setup an alias:

  1. Press SETTING and navigate to the Alias Codes tab.
  2. Press EMERGENCY STOP on the control.
  3. Using the cursor keys select the M or G Macro Call to be used.
  4. Enter the number of the G-code or M-code you want to alias. For example, if you want to alias G06 type 06.
  5. Press ENTER.
  6. Repeat steps 3 - 5 for other aliased G or M-codes.
  7. Release the EMERGENCY STOP on the control.

    Setting an alias value to 0 disables aliasing for the associated subprogram.

    Alias Codes Window

Be aware: Many service and repair procedures should be done only by authorized personnel. The service technicians at your Haas Factory Outlet (HFO) have the training, experience, and are certified to do these tasks safely and correctly. You should not do machine repair or service procedures unless you are qualified and knowledgeable about the processes.

Danger: Some service procedures can be dangerous or life-threatening. DO NOT attempt a procedure that you do not completely understand. Contact your Haas Factory Outlet (HFO) and schedule a service technician visit if you have any doubts about doing a procedure.

Feedback