Rotary Model Selection

Next Generation Control Mill Operator's Manual

The Online Interactive Operator's Manual is currently available in English only.

A PDF version of the Operator's Manual is available for download in multiple languages. Click the link below to view the Operator's Manual in your language. Click "Continue" to view the online version in English.

Get a translated PDF Download Continue

In this procedure, you select your particular rotary model from the list of models in the control, so that the control can load the correct parameters for that unit. In this example, we have a TR160 unit installed on the table, with the tilt axis parallel to X.

We want to configure both the rotary (platter) and tilt (trunnion) axes. The rotary axis is physically connected to the 5th axis at the control cabinet. We want to designate the rotary axis C. The tilt axis is physically connected to the 4th axis at the control cabinet. We want to designate the tilt axis A.

  1. Find the nameplate on your rotary unit. Record the values in the “MODEL NO.” (model number) and “VER” (version) fields. On our example nameplate, we find that the model number is TR160, and the version is P4.

    Example rotary nameplate. [1] Model Number, [2] Version

     

  2. On the Rotary Selection page, use the CURSOR keys or the jog handle to browse the list of rotary models to find your model.

    Dual-axis rotary units have two entries in the list: one for the rotary axis (ROT), and one for the tilt axis (TLT). Be sure to select the rotary model that matches both the model number and version on the nameplate. In the example below, the cursor highlights the rotary axis of the model that matches our example nameplate (TR160-P4-ROT).

    Rotary Selection Example. [1] Model Column, [2] Name Column, [3] Fifth Axis Column, [4] Fourth Axis Column, [5] Current Selection (Highlighted).

  3. Press ENTER. The Select Table Orientation window appears.

    The Select Table Orientation Window. [1] Orientation Example Image, [2] Axis Configuration (Letter Assignment), [3] Physical Connection, [4] The Rotary Configuration Must Match the Picture to use TCPC/DWO.

  4. Press A, B, or C to change the axis letter.
  5. Press F4 to toggle the physical connection setting between 4th and 5th.
  6. Press ENTER to save the configuration to the Select New Rotaries table, or press UNDO to cancel.
  7. Repeat steps 2-6 for the tilt axis, if applicable. In this example, we would now set up the TR160 tilt axis (TR160-P4-TLT).
  8. After you complete the axis configuration, press EMERGENCY STOP, and then press F3 to apply the rotary parameters.
  9. Cycle power.

Be aware: Many service and repair procedures should be done only by authorized personnel. The service technicians at your Haas Factory Outlet (HFO) have the training, experience, and are certified to do these tasks safely and correctly. You should not do machine repair or service procedures unless you are qualified and knowledgeable about the processes.

Danger: Some service procedures can be dangerous or life-threatening. DO NOT attempt a procedure that you do not completely understand. Contact your Haas Factory Outlet (HFO) and schedule a service technician visit if you have any doubts about doing a procedure.

Feedback