Restoring Selected Backups

Next Generation Control Mill Operator's Manual

The Online Interactive Operator's Manual is currently available in English only.

A PDF version of the Operator's Manual is available for download in multiple languages. Click the link below to view the Operator's Manual in your language. Click "Continue" to view the online version in English.

Get a translated PDF Download Continue

This procedure tells you how to restore selected data backups from a USB memory device.

  1. Insert the USB memory device with the backup files into the USB port on the right side of the control pendant.
  2. Navigate to USB in the Device Manager.
  3. Press EMERGENCY STOP.
  4. Open the directory that contains the files you want to restore.
  5. Highlight or type in the name of the file to be restored. Typed file name takes precedence over highlighted file name.
    note: Type the backup name with or without a file extension (e.g., MACROS or MACROS.VAR)
  6. Press F4.
  7. Highlight the backup type to load and press ENTER.

    The highlighted file or the typed name file is loaded on the machine. The message Disk Done displays after loading is complete.

    note: Settings load the moment you pick Settings from the System [F4] drop-down menu. Highlighting or typing is not required.

Be aware: Many service and repair procedures should be done only by authorized personnel. The service technicians at your Haas Factory Outlet (HFO) have the training, experience, and are certified to do these tasks safely and correctly. You should not do machine repair or service procedures unless you are qualified and knowledgeable about the processes.

Danger: Some service procedures can be dangerous or life-threatening. DO NOT attempt a procedure that you do not completely understand. Contact your Haas Factory Outlet (HFO) and schedule a service technician visit if you have any doubts about doing a procedure.

Feedback