Restoring From a Backup

Classic Control - Mill Operator's Manual

The Online Interactive Operator's Manual is currently available in English only.

A PDF version of the Operator's Manual is available for download in multiple languages. Click the link below to view the Operator's Manual in your language. Click "Continue" to view the online version in English.

Get a translated PDF Download Continue

This procedure tells you how to restore your machine data from the backup on a USB memory device.

  1. Insert the USB memory device with the backup files into the USB port on the right side of the control pendant.
  2. Select the USB tab in the Device Manager.
  3. Press EMERGENCY STOP.
  4. Open the directory that contains the files you want to restore.
  5. Press F4.

    The Save and Load pop-up menu appears.

  6. Highlight Load All - Restore to load all file types (settings, parameters, programs, macros, tool offsets, variables, etc.)
  7. Type the backup name with no extension (e.g., 28012014) that you want to restore, and press ENTER.

    All the files with the typed backup name are loaded on the machine. The message “Disk Done” displays after loading is complete.

  8. To load a specific file type (like name.PAR for parameters), press F4, highlight the file type (in this case, Load Parameters), type the backup name with no extension, and then press ENTER.

    The file with the typed backup name (in this case name.PAR) is loaded on the machine. The message “Disk Done” displays after loading is complete.

Be aware: Many service and repair procedures should be done only by authorized personnel. The service technicians at your Haas Factory Outlet (HFO) have the training, experience, and are certified to do these tasks safely and correctly. You should not do machine repair or service procedures unless you are qualified and knowledgeable about the processes.

Danger: Some service procedures can be dangerous or life-threatening. DO NOT attempt a procedure that you do not completely understand. Contact your Haas Factory Outlet (HFO) and schedule a service technician visit if you have any doubts about doing a procedure.

Feedback