Run-Stop-Jog-Continue

Run-Stop-Jog-Continue (RSJC) is a control feature available on Haas mills and lathes for software versions M11.02 and L9.02 and higher.

This feature lets you to stop a program that is in operation, jog away from the part, and then continue the program. After the tool is away from the part, you can replace a worn insert or broken tool or examine an important part feature. You can then continue the program again.

caution: When the program continues, it uses the OFFSET values from the OFFSET page, and the machine does not go back through the same path that you jogged away. If you replace tools, the length must be the same as the tool before.

Refer to your Operator's Manual for more information about this function.

Be aware: Many service and repair procedures should be done only by authorized personnel. The service technicians at your Haas Factory Outlet (HFO) have the training, experience, and are certified to do these tasks safely and correctly. You should not do machine repair or service procedures unless you are qualified and knowledgeable about the processes.

Danger: Some service procedures can be dangerous or life-threatening. DO NOT attempt a procedure that you do not completely understand. Contact your Haas Factory Outlet (HFO) and schedule a service technician visit if you have any doubts about doing a procedure.

Feedback