Next Generation Control - Networking Option - Icons

Introduction

This document tells you the meaning of the networking icons that are shown in the status bar [1] of the control for machines that have the Next Generation Control.
Next Generation Control - Networking Option - Icons
Icon Description
The machine is connected to the internet via a wired network with an Ethernet cable.
The machine is connected to the internet via a wireless network and has 70 - 100% signal strength.
The machine is connected to the internet via a wireless network and has 30 - 70% signal strength.
The machine is connected to the internet via a wireless network and has 1 - 30% signal strength.
The machine was connected to the internet via a wireless network and is not receiving any data packets.
The machine is successfully registered with HaasConnnect and is communicating with the server.
The machine had previously registered with HaasConnect and has a problem connecting to the server.
The machine is connected to a remote Netshare.

Be aware: Many service and repair procedures should be done only by authorized personnel. The service technicians at your Haas Factory Outlet (HFO) have the training, experience, and are certified to do these tasks safely and correctly. You should not do machine repair or service procedures unless you are qualified and knowledgeable about the processes.

Danger: Some service procedures can be dangerous or life-threatening. DO NOT attempt a procedure that you do not completely understand. Contact your Haas Factory Outlet (HFO) and schedule a service technician visit if you have any doubts about doing a procedure.

Feedback