Standard Coolant - Filter - Maintenance

Applies to machines built from: 
December, 2011 to April, 2014

Standard Coolant System - Filter - Maintenance

The filter for the standard coolant system has a container. Chips and debris collect at the bottom of the container. This procedure tells you how to do these tasks:
  1. Clean the container.
  2. Clean the filter.
  3. Lubricate the container.
  4. Lubricate the o-ring.

Step 1

Use the supplied wrench [2] to remove the filter container [1].

Remove all of the chips and coolant from the container.

Fully clean the container [3].

Step 2

Use compressed air [3] to blow chips and debris from the filter element [2].

Blow debris out of the inner surface of the filter head [1].

Find the surface [4] where the o-ring on the installed container will touch the filter head.

Fully clean this area.

Use a towel that is soft and clean.

caution: Make sure to clean all debris from this surface. Debris causes leaks.

Apply a thin layer of silicone grease [5] to the clean surface.

Step 3

Fully clean the o-ring [1].

Fully clean the o-ring groove [2].

Examine the o-ring.

If the o-ring is cracked or broken [3], replace it.

Apply a thin layer of silicone grease to these areas:

  • the o-ring [4]
  • the o-ring groove [5]
  • the threads [6] on the filter container

Put the o-ring into the o-ring groove.

Make sure the o-ring is installed tightly in position.

Step 4

Align the filter container with the filter head [1].

Carefully turn the filter container with your hand into the head.

caution: Do not use the wrench [2].

Turn the container until it is tight.

Loosen the container 1/4 of a turn.

Press COOLNT to start the coolant system.

Monitor the filter head for leaks.

If the filter has leaks, do steps 1-4 again.

Be aware: Many service and repair procedures should be done only by authorized personnel. The service technicians at your Haas Factory Outlet (HFO) have the training, experience, and are certified to do these tasks safely and correctly. You should not do machine repair or service procedures unless you are qualified and knowledgeable about the processes.

Danger: Some service procedures can be dangerous or life-threatening. DO NOT attempt a procedure that you do not completely understand. Contact your Haas Factory Outlet (HFO) and schedule a service technician visit if you have any doubts about doing a procedure.

Feedback