Side Mount (SMTC) - EC-Series - Cambox - Maintenance

Applies to machines built from: 
January, 2003

EC Series - SMTC - Cambox - Maintenance

This procedure tells you how to make sure the cambox has the correct oil level.
Push POWER OFF. Set the main circuit breaker to the OFF position. Lock the main circuit breaker. Use an approved lock with an approved safety tag.
Remove the oil level plug [1]. If the oil level is correct, oil will come out of the oil level plug hole. If oil does not come out, leave the plug off.

Do these steps if the oil level is not correct:

Remove the breather [2] from the hose [3] (or fitting). Make sure that the hose has no low points and is not kinked.

Add Mobil 15w-50 through the hose [3] in small increments until oil comes out of the oil level plug [1] hole.

Install the oil level plug [1] and the breather [2].

Tools Required

Mobil 15w-50

Be aware: Many service and repair procedures should be done only by authorized personnel. The service technicians at your Haas Factory Outlet (HFO) have the training, experience, and are certified to do these tasks safely and correctly. You should not do machine repair or service procedures unless you are qualified and knowledgeable about the processes.

Danger: Some service procedures can be dangerous or life-threatening. DO NOT attempt a procedure that you do not completely understand. Contact your Haas Factory Outlet (HFO) and schedule a service technician visit if you have any doubts about doing a procedure.

Feedback