Next Generation Control - Net Share - Local

A Local Net Share connection gives computers on the network access to the control's User Data directory.

Step 1

Make sure Local Net Share Enabled [1] is set to On.

Make sure you enter a Local Password [2].

note: Use this password on the computer to access the User Data directory.

Push F4 to apply changes.

Step 2

Get the IP Address [1] of the connection.

This is in the Wired Connection tab or Wireless Connection tab.

Step 3

On a computer on the network, use the Start menu to open a Run [1] command.

Enter the IP Address from the machine in the format shown [2]. Select OK [3].

The Windows Security prompt shows.

Type haas [4] for the user name.

Type your Local Password [5].

Select OK [6].

Step 4

A folder named User Data [1] opens.

The files [2] in the User Data [1] folder are the same files [4] that are in the User Data [3] directory on the control.

Be aware: Many service and repair procedures should be done only by authorized personnel. The service technicians at your Haas Factory Outlet (HFO) have the training, experience, and are certified to do these tasks safely and correctly. You should not do machine repair or service procedures unless you are qualified and knowledgeable about the processes.

Danger: Some service procedures can be dangerous or life-threatening. DO NOT attempt a procedure that you do not completely understand. Contact your Haas Factory Outlet (HFO) and schedule a service technician visit if you have any doubts about doing a procedure.

Feedback