Classic Haas Control (CHC) - DHCP Network Connection

Applies to machines built from: 
January, 2010

Connecting to a Network using DHCP

This procedure tells you how to configure the Haas machine to connect to a computer network with DHCP enabled. This allows the CNC machine to get its IP address automatically. This configuration is for example only; the setting values required to connect to your network may be different. Contact your network administrator for the exact settings.

Step 1

To enable networking, make sure Parameters 737:10 ENABLE HARD DRIVE and 737:11 ENABLE NETWORKING are set to 1 (enabled).

note: These parameters require an unlocked code to enable.

Step 2

  • Setting 900 [1] is the name which identifies the CNC machine as a device on the network. Each machine must have a unique CNC network name. The name cannot be longer than (8) characters.
  • Setting 901 [2] toggles the automatic IP feature. Change Setting 901 [2] to ON.
  • Settings 902, 903, 904, 905 and 906 [3] are the network addresses and settings that the control uses to communicate on your network. They are set automatically by Setting 901 when it is enabled.
  • Settings 907 through 910 [4] are used for advanced network configuration. Normally, these are left empty.
  • Setting 911 [5] sets the amount of access the wireless network has to the files on the CNC machine. Normally, this is set to FULL.

Be aware: Many service and repair procedures should be done only by authorized personnel. The service technicians at your Haas Factory Outlet (HFO) have the training, experience, and are certified to do these tasks safely and correctly. You should not do machine repair or service procedures unless you are qualified and knowledgeable about the processes.

Danger: Some service procedures can be dangerous or life-threatening. DO NOT attempt a procedure that you do not completely understand. Contact your Haas Factory Outlet (HFO) and schedule a service technician visit if you have any doubts about doing a procedure.

Feedback