Axis Servo Motor Cable - Brushless - With Grommet - Replacement

Control - Axis Motor Cable - Brushless - With Grommet - Replacement

This procedure tells you how to replace these brushless axis cables:
  • 2-Cable set: motor power and encoder
  • 3-Cable set: motor power, encoder, and brake
Safety Notes
Caution: When you do maintenance or repair on CNC machines and their components, you must always follow basic safety precautions. This decreases the risk of injury and mechanical damage.

Do these steps before you do work in the machine or in the control cabinet:
  • Set the main circuit breaker to the OFF position.
  • Use an approved lock with an approved safety tag. Always follow lock-out procedures in accordance to local government rules.
  • After turning off the machine, wait at least 5 minutes before working in the control cabinet, to allow power to dissipate. Wait for the voltage indicator LED on the vector drive to go off completely.
  • Always turn off the main air supply when you work on any part of the pneumatic system.
  • Make sure to rest the spindle head on a block of wood when work is done on a vertical axis. This will prevent any unintended movement that could result in the axis falling.
  • Never alter any safety circuits on the machine.
You should not do machine repair or service procedures unless you are qualified and knowledgeable about the processes. Serious damage to the machine components can result in costly repairs. The service technicians at your Haas Factory Outlet (HFO) have the training and experience, and are certified to do these tasks safely and correctly. The repair and service work performed by your HFO is protected with a limited warranty.
danger: Some service procedures can be dangerous or life-threatening. DO NOT attempt a procedure that you do not fully understand. If you have any doubts about doing a procedure contact your Haas Factory Outlet (HFO) and schedule a service visit.

Tools Required

Di-electric Grease

Step 1

Push POWER OFF. Set the main circuit breaker to the OFF position. Lock the main circuit breaker. Use an approved lock with an approved safety tag.

Step 2

note: The replacement cable kit includes a grommet. The grommet has holes for the Power Cable [1], Encoder Cable [2], and [3] Brake Cables (The brake cable hole [3] is not on the grommet if you have a 2-Cable set).

If the cable that you must replace has a mechanical axis limit switch cable [4] for the axis movement, install the jumper [5] on the switch cable [4].

Step 3

Put labels on the locations of the cables you will replace.

  • The encoder cable connection location is on the processor PCB [1]
  • The power cable connection location is on the amplifier [2]
  • If you have a brake cable, the connection location is on the I/O PCB [3]

Cut the extra rubber [3] off of the grommet. Make sure a space is between the smaller diameter of the grommet and the larger diameter of the grommet, as shown [4].

Fill the amphenol connectors on the motors [5] with dielectric grease.

Install the new axis cable. Put the cables [6] into the grommet [7]. If you have a brake cable, put it in the grommet [7] first.

Push the grommet [7] through the hole in the control cabinet. Make sure the tab [8] on the grommet goes fully through. This holds the grommet in position on the inside of the control cabinet.

Be aware: Many service and repair procedures should be done only by authorized personnel. The service technicians at your Haas Factory Outlet (HFO) have the training, experience, and are certified to do these tasks safely and correctly. You should not do machine repair or service procedures unless you are qualified and knowledgeable about the processes.

Danger: Some service procedures can be dangerous or life-threatening. DO NOT attempt a procedure that you do not completely understand. Contact your Haas Factory Outlet (HFO) and schedule a service technician visit if you have any doubts about doing a procedure.

Feedback