HaasConnect - Machine Registration

On the Machine
  1. Press SETTING.
  2. Select the Network tab.
  3. Select the HaasConnect sub-tab.
  4. Press F1.
  5. Press ENTER to accept the disclaimer.

    The HaasConnect screen shows the machine serial number and a PIN code. Record these numbers.

On the HaasConnect Website
  1. Log in to HaasConnect.
  2. Put your mouse cursor over My Machines and click Add New Machine.

  3. Fill in the fields with the machine serial number, PIN code, and a nickname. A descriptive nickname can help you quickly identify the machine in the list.

  4. Click Submit.
  5. Select the initial notifications you want to receive for this machine, and then select Continue. You can change your selections later; refer to the Administrator's Guide for more information.
  6. Select the notification method for the user(s) who will receive notifications about this machine. Remember that you can only send text messages to verified mobile telephone numbers. You can change your selections later; refer to the Administrator's Guide for more information.
On the Machine
  1. When the machine and HaasConnect first begin communicating, a connection success screen is shown.

  2. The machine is shown on your list of machines on the HaasConnect website, and you can adjust the notification settings on the site. Refer to the Administrator's Guide for more information about notification setup.

Be aware: Many service and repair procedures should be done only by authorized personnel. The service technicians at your Haas Factory Outlet (HFO) have the training, experience, and are certified to do these tasks safely and correctly. You should not do machine repair or service procedures unless you are qualified and knowledgeable about the processes.

Danger: Some service procedures can be dangerous or life-threatening. DO NOT attempt a procedure that you do not completely understand. Contact your Haas Factory Outlet (HFO) and schedule a service technician visit if you have any doubts about doing a procedure.

Feedback