Coolant Refill - Calibration

Applies to machines built from: 
April, 2015
Classic Haas Control - Coolant Refill - Calibration

  1. Push CURNT COMDS. Push PAGE DOWN until the Coolant Refill screen shows [1].
  2. Fill the Coolant Refill container with 5 gallons of coolant concentrate.
  3. Push F4 [4] to set the Max gal. coolant added before replenishing concentrate. Push Y.
  4. Remove the filler hose from the filler pipe.
  5. Put a bucket [5] under the filler pipe.
  6. F3starts the coolant flow.
  7. F3stops the coolant flow.
  8. Push F3 to fill the bucket. Push F3 again to stop when the coolant mixture fills the bucket.
  9. Measure the concentration of the coolant. Refer to the Maintaining Your Coolant Mixture video.
  10. If the measured concentration is lower than the value for the Coolant Concentration Percent [2], increase the value for the Coolant Concentration Adjust [3].
  11. If the concentration is higher than the value for the Coolant Concentration Percent [2], decrease the value for the Coolant Concentration Adjust [3].
  12. Repeat the measurements until the concentration matches the value for Coolant Concentration Percent [2].
Next Generation Control - Coolant Refill - Calibration

  1. Push DIAGNOSTIC.

    Push the RIGHT CURSOR arrows to select the Maintenance tab.

    Push the DOWN and RIGHT CURSOR arrows to select the Coolant Refill tab.

  2. Fill the Coolant Refill container with 5 gallons of coolant concentrate.
  3. Push F4 to set the Maximum Coolant From Remaining Concentrate.

    Push Y.

  4. Remove the filler hose from the filler pipe.
  5. Put a bucket under the filler pipe.
  6. F3 starts the coolant flow.
  7. F3 stops the coolant flow.
  8. Push F3 to fill the bucket.

    Push F3 again to stop when the coolant mixture fills the bucket.

  9. Measure the concentration of the coolant. Refer to the Maintaining Your Coolant Mixture video.
  10. If the measured concentration is lower than the value for the Coolant Concentrate [1], increase the value for the Concentrate Adjustment [2].
  11. If the concentration is higher than the value for the Coolant Concentrate [1], decrease the value for the Concentrate Adjustment [2].
  12. Repeat the measurements until the concentration matches the value for Coolant Concentrate [1].
Coolant Refill - Filler Hose - Installation

Install the part as shown.

  • Filler Hose [2] - Install to the filler pipe [1].
    caution: Make sure the Filler Hose does not touch the coolant [3].

Be aware: Many service and repair procedures should be done only by authorized personnel. The service technicians at your Haas Factory Outlet (HFO) have the training, experience, and are certified to do these tasks safely and correctly. You should not do machine repair or service procedures unless you are qualified and knowledgeable about the processes.

Danger: Some service procedures can be dangerous or life-threatening. DO NOT attempt a procedure that you do not completely understand. Contact your Haas Factory Outlet (HFO) and schedule a service technician visit if you have any doubts about doing a procedure.

Feedback