Classic Haas Control (CHC) - Wireless Network Bridge

Applies to machines built from: 
August, 2009
This document gives an overview of the use of a wireless network bridge with Haas machines.

If you have the Ethernet option, you can connect your Haas machine to your wireless network with a wireless network bridge. Follow the bridge manufacturer's instructions to connect the bridge to your wireless network.

note: You can use the 120V power outlet on the side of the machine's control cabinet to power the bridge.

 

This is an example diagram of a wireless bridge setup. [1] Wireless Network Bridge, [2] Wired Connection between the Haas Machine and the Bridge, [3] Wireless Network Bridge Power Connection

CNC Network Connection Settings

This procedure tells you how to connect the Haas machine to your network.

Be aware: Many service and repair procedures should be done only by authorized personnel. The service technicians at your Haas Factory Outlet (HFO) have the training, experience, and are certified to do these tasks safely and correctly. You should not do machine repair or service procedures unless you are qualified and knowledgeable about the processes.

Danger: Some service procedures can be dangerous or life-threatening. DO NOT attempt a procedure that you do not completely understand. Contact your Haas Factory Outlet (HFO) and schedule a service technician visit if you have any doubts about doing a procedure.

Feedback