Background Editor - Change a Program Code During a Program Operation


General Information

While a program operates, you can change the program code. Or you can change the code of a different program that is in MEMORY.

Change the Code of a Program in Operation

  1. While the program operates, press EDIT. BACKGROUND EDITOR shows at the top of the display.
  2. Make changes to the program.
  3. To go back to the program in operation, press PROGRAM.
note: The changes have no effect on the program in operation. You see the changes when you open or operate the program again.

Change the Code of a Different Program in MEMORY

  1. While the program operates, press EDIT.
  2. Press SELECT PROGRAM.
  3. Press the UP or DOWN CURSOR arrow to select a program.
  4. Press WRITE/ENTER.
  5. Make changes to the program.
  6. To go back to the program in operation, press PROGRAM.

Be aware: Many service and repair procedures should be done only by authorized personnel. The service technicians at your Haas Factory Outlet (HFO) have the training, experience, and are certified to do these tasks safely and correctly. You should not do machine repair or service procedures unless you are qualified and knowledgeable about the processes.

Danger: Some service procedures can be dangerous or life-threatening. DO NOT attempt a procedure that you do not completely understand. Contact your Haas Factory Outlet (HFO) and schedule a service technician visit if you have any doubts about doing a procedure.

Feedback