Offsets

Classic Control - Mill Operator's Manual

The Online Interactive Operator's Manual is currently available in English only.

A PDF version of the Operator's Manual is available for download in multiple languages. Click the link below to view the Operator's Manual in your language. Click "Continue" to view the online version in English.

Get a translated PDF Download Continue

The work-offset display is found on the OFFSET display. The G54 through G59 or G110 through G129 offsets can be set by using the PART ZERO SET button. This will work with only the work zero offsets display selected.

  1. Press OFFSET and navigate to the WORK ZERO OFFSET tab.
  2. Position the axes to the work zero point of the workpiece.
  3. Using the cursor, select the proper axis and work number.
  4. Press PART ZERO SET and the current machine position is automatically stored in that address.
  5. note: Entering a nonzero Z work offset will interfere with the operation of an automatically entered tool length offset.
    Work coordinate numbers are usually entered as positive numbers. Work coordinates are entered into the table as a number only. To enter an X value of X2.00 into G54, cursor to the X column and enter 2.0.

Be aware: Many service and repair procedures should be done only by authorized personnel. The service technicians at your Haas Factory Outlet (HFO) have the training, experience, and are certified to do these tasks safely and correctly. You should not do machine repair or service procedures unless you are qualified and knowledgeable about the processes.

Danger: Some service procedures can be dangerous or life-threatening. DO NOT attempt a procedure that you do not completely understand. Contact your Haas Factory Outlet (HFO) and schedule a service technician visit if you have any doubts about doing a procedure.

Feedback