Fadal Program Converter

Classic Control - Mill Operator's Manual

The Online Interactive Operator's Manual is currently available in English only.

A PDF version of the Operator's Manual is available for download in multiple languages. Click the link below to view the Operator's Manual in your language. Click "Continue" to view the online version in English.

Get a translated PDF Download Continue

If you need to convert a program from Fadal format to Haas, The Fadal Program Converter lets you do so quickly.

Load FADAL Popup

Fadal Conversion Complete

Fadal Conversion Errors

  1. Press LIST PROGRAM to access the converter.
  2. Highlight the Fadal program.
  3. Press F1.
  4. Select Load FADAL from the pop-up menu.

    The control loads the converted program into memory. A copy of the converted program is also saved to the current storage device, with an “.out” extension. This file has Converted Fadal Program at the top to confirm that it is a converted program. Any lines that could not be converted are commented out with an M199, which will give a User Generated Alarm when the program is run. Edit these lines for Haas compatibility.

    tip:

    You can use the search function in EDIT mode to quickly find unconverted lines. With the converted program in the active pane (press PROGRAM to change the active pane), press F1 or HELP and select Search from the pop-up menu. Use M199 as the search term.

Be aware: Many service and repair procedures should be done only by authorized personnel. The service technicians at your Haas Factory Outlet (HFO) have the training, experience, and are certified to do these tasks safely and correctly. You should not do machine repair or service procedures unless you are qualified and knowledgeable about the processes.

Danger: Some service procedures can be dangerous or life-threatening. DO NOT attempt a procedure that you do not completely understand. Contact your Haas Factory Outlet (HFO) and schedule a service technician visit if you have any doubts about doing a procedure.

Feedback