Control Icon Guide

Classic Control - Mill Operator's Manual

The Online Interactive Operator's Manual is currently available in English only.

A PDF version of the Operator's Manual is available for download in multiple languages. Click the link below to view the Operator's Manual in your language. Click "Continue" to view the online version in English.

Get a translated PDF Download Continue
Name Icon Meaning
SETUP KEY LOCKED Setup mode is locked; the control is in “Run” mode. Most machine functions are disabled or limited while the machine doors are open.
SETUP KEY UNLOCKED Setup mode is unlocked; the control is in “Setup” mode. Most machine functions are available, but may be limited, while the machine doors are open.
DOOR HOLD Machine motion has stopped because of door rules.
RUNNING The machine is running a program.
JOGGING An axis is jogging at the current jog rate.
POWER SAVING SERVOS OFF The power-saving servos off feature is active. Servos are turned off. Press a key to activate the servos.
JOG RETURN This icon appears while the control returns to the workpiece during a run-stop-jog-continue operation.
JOG HOLD You have pressed FEED HOLD during the return portion of a run-stop-jog-continue operation.
JOG AWAY This icon prompts you to jog away during a run-stop-jog-continue operation.
RESTART The control scans the program before a restart if Setting 36 is ON.
SINGBK STOP SINGLE BLOCK mode is active, and the control needs a command to continue.
FEEDHOLD The machine is in feed hold. Axis motion has stopped, but the spindle continues to turn.
FEED The machine is executing a cutting move.
RAPID The machine is executing a non-cutting axis move ( G00) at the fastest possible rate.
DWELL The machine is executing a dwell ( G04) command.
JOG LOCK ON Jog lock is active. If you press an axis key, that axis moves at the current jog rate until you press JOG LOCK again, or the axis reaches its limit.
REMOTE JOG The optional remote jog handle is active.
VECTOR JOG For gimbaled spindle mills, the tool will jog along the vector defined by the position of the spindle rotary positions.
X MIRROR Mirroring mode ( G101) is active in the positive direction. The icon message includes the currently mirrored axes.
AXIS UNCLAMPED A rotary axis, or a combination of rotary axes, is unclamped. The icon message includes the axes that are currently unclamped.
WARNING LOW VOLTAGE Power Fault Detect Module (PFDM) Incoming Voltage is under the nominal operating level.
WARNING HIGH VOLTAGE PFDM Incoming Voltage is above the nominal operating level.
ALARM HIGH VOLTAGE PFDM Incoming Voltage is above the nominal operating level.
ALARM LOW AIR PRESSURE System air pressure is critically low.
WARNING LOW AIR PRESSURE System air pressure is low.
WARNING HIGH AIR PRESSURE System air pressure ishigh.
ALARM HIGH AIR PRESSURE System air pressure is critically high
LOW GEAR BOX OIL FLOW LOW GEAR BOX OIL LEVEL The spindle gear box oil level is low.
CHECK ROTARY LUBRICATION LEVEL The rotary table lubrication oil reservoir needs service, or the rotary table brake fluid needs service.
DIRTY TSC FILTER The Through Spindle Coolant filter needs service.
LOW COOLANT CONCENTRATE The concentrate reservoir for the coolant refill system needs service.
LOW SPINDLE OIL LEVEL LOW SECOND SPINDLE OIL LOW GREASE LEVEL The spindle lubrication oil system detected a low oil condition, or the axis ball screw lubrication system detected a low grease or low pressure condition. Refer to the note after this table.
LOW ROTARY BRAKE FLUID The rotary brake fluid reservoir needs service.
MAINTENANCE DUE A maintenance procedure is due, based on information in the MAINTENANCE page. The maintenance page is part of Current Commands.
EMERGENCY STOP, PENDANT EMERGENCY STOP on the pendant has been pressed. This icon disappears when EMERGENCY STOP is released.

EMERGENCY STOP, PALLET

EMERGENCY STOP on the pallet changer has been pressed. This icon disappears when EMERGENCY STOP is released.

EMERGENCY STOP, TC CAGE

EMERGENCY STOP on the tool changer cage has been pressed. This icon disappears when EMERGENCY STOP is released.

EMERGENCY STOP, AUXILIARY

EMERGENCY STOP on an auxiliary device has been pressed. This icon disappears when EMERGENCY STOP is released.
SINGLE BLOCK SINGLE BLOCK mode is active. The control executes programs (1) block at a time, and you need to press CYCLE START to execute the next block.
DRY RUN DRY RUN mode is active.
OPTION STOP OPTIONAL STOP is active. The control stops the program at each M01 command.
BLOCK DELETE BLOCK DELETE is active. The control skips program blocks that begin with a slash (/).
CAGE OPEN The side-mount tool changer door is open.
TOOL CHANGER MANUAL CCW The side-mount tool changer carousel is turning counter-clockwise as commanded by a manual carousel rotation button.
TOOL CHANGER MANUAL CW The side-mount tool changer carousel is turning clockwise as commanded by a manual carousel rotation button.
TOOL CHANGE A tool change is in progress.
TOOL UNCLAMPED The tool in the spindle is unclamped.
CONVEYOR FORWARD The conveyor is active and currently moving forward.
CONVEYOR REVERSE The conveyor is active and currently moving in reverse.
TSC ON The Through-Spindle Coolant (TSC) system is active.
TAB ON The Tool Air Blast (TAB) system is active.
AIR BLAST ON The Auto Air Gun is active.
COOLANT ON The main coolant system is active.
COOLANT REFILL ON The Coolant Refill feature is mixing and adding coolant to the tank.

Be aware: Many service and repair procedures should be done only by authorized personnel. The service technicians at your Haas Factory Outlet (HFO) have the training, experience, and are certified to do these tasks safely and correctly. You should not do machine repair or service procedures unless you are qualified and knowledgeable about the processes.

Danger: Some service procedures can be dangerous or life-threatening. DO NOT attempt a procedure that you do not completely understand. Contact your Haas Factory Outlet (HFO) and schedule a service technician visit if you have any doubts about doing a procedure.

Feedback