Circle-Circle-Tangent Sub-tab

Classic Control - Mill Operator's Manual

The Online Interactive Operator's Manual is currently available in English only.

A PDF version of the Operator's Manual is available for download in multiple languages. Click the link below to view the Operator's Manual in your language. Click "Continue" to view the online version in English.

Get a translated PDF Download Continue

This feature determines points of intersection between two circles or points. You provide the location of two circles and their radii. The control calculates the intersection points that are formed by lines tangent to both circles.

note: For every input condition (two disjointed circles), there are up to eight intersection points. Four points are from drawing straight tangents and four points by forming cross tangents.
  1. Use the UP and DOWN cursor arrows to highlight the data field for the value you want to enter.
  2. Type the value and press ENTER.

    After you enter the required values, the control displays the tangent coordinates and associated straight type diagram.

  3. Press F1 to toggle between straight and cross tangent results.
  4. Press F and the control prompts for the From and To points (A, B, C, etc.) that specify a segment of the diagram. If the segment is an arc, the control will also prompt for C or W (CW or CCW). To quickly change segment selection, press T to make the previous To point become the new From point and the control prompts for a new To point.

    The Input Bar displays the G code for the segment. Solution is in G90 mode. Press M to toggle to G91 mode.

  5. Press MDI DNC or EDIT and press INSERT to enter the G-code from the Input Bar.

Calculator Circle-Circle-Tangent Type: Straight Example

This example creates this G-code on the input line. From: A To: C generates:

G01 X-4.346 Y-3.7565

Calculator Circle-Circle-Tangent Type: Cross Example

Be aware: Many service and repair procedures should be done only by authorized personnel. The service technicians at your Haas Factory Outlet (HFO) have the training, experience, and are certified to do these tasks safely and correctly. You should not do machine repair or service procedures unless you are qualified and knowledgeable about the processes.

Danger: Some service procedures can be dangerous or life-threatening. DO NOT attempt a procedure that you do not completely understand. Contact your Haas Factory Outlet (HFO) and schedule a service technician visit if you have any doubts about doing a procedure.

Feedback