Alarm Alerts

Classic Control - Mill Operator's Manual

The Online Interactive Operator's Manual is currently available in English only.

A PDF version of the Operator's Manual is available for download in multiple languages. Click the link below to view the Operator's Manual in your language. Click "Continue" to view the online version in English.

Get a translated PDF Download Continue

Haas machines include a basic application to send an alert to an email address or cellular telephone when an alarm occurs. Setting up this application requires some knowledge about your network; ask your system administrator or Internet Service Provider (ISP) if you do not know the correct settings.

Before you set up alerts, make sure the machine has an established connection to your Local Area Network, and that Setting 900 defines a unique network name for the machine. This feature requires the Ethernet option and software version 18.01 or later.

  1. Using an Internet browser on another device connected to the network, type the machine’s network name (Setting 900) into the browser address bar and press ENTER.
  2. A message may appear with a request to set a cookie in your browser. This will happen each time you access the machine using a different computer or browser, or after an existing cookie has expired. Click OK.
  3. The home screen displays, with the setup options at the bottom of the screen. Click Manage Alerts.
  4. At the Manage Alerts screen, enter the email address and/or cellular phone number where you want to receive alerts. If you enter a cellular phone number, select your carrier from the pull-down menu under the cell number field. Click SUBMIT CHANGES.
  5. note: If your cellular carrier is not listed in the menu, ask your carrier to provide your account’s email address through which you can receive text messages. Enter this address in the email field.
    Click Configure Email Interface.
  6. note: Haas Automation service personnel cannot diagnose or repair problems with your network.
    Fill in the fields with your email system’s information. Ask your system administrator or ISP if you do not know the correct values. Click the Submit Changes button when finished. In the first field, enter the IP address for your domain name server (DNS). In the second field, enter your simple mail transfer protocol (SMTP) server name. The third field, SMTP server port, is already populated with the most common value (25). Change this only if the default setting does not work. In the last field, enter an authorized email address, which the application will use to send the alert.
  7. Press EMERGENCY STOP to generate an alarm to test the system. An email or text message should arrive at the designated address or telephone number with details about the alarm.

Be aware: Many service and repair procedures should be done only by authorized personnel. The service technicians at your Haas Factory Outlet (HFO) have the training, experience, and are certified to do these tasks safely and correctly. You should not do machine repair or service procedures unless you are qualified and knowledgeable about the processes.

Danger: Some service procedures can be dangerous or life-threatening. DO NOT attempt a procedure that you do not completely understand. Contact your Haas Factory Outlet (HFO) and schedule a service technician visit if you have any doubts about doing a procedure.

Feedback